This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: epwm:

Part Number: TMS320F28377D

On the maximum clock frequency of epwm:

After reading the specification, it is clearly stipulated that the maximum clock of epwm can only be 100MHz (premise of main frequency 200MHz),

If my system needs 60K frequency, that is, the number of PWM is 1666, and the system voltage is 200V,

That is to say, the PWM resolution is only 120mV, which is a bit low. What can I do to improve this resolution?