This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000WARE: how can I set the motor PWM sequence if I got the hall sensor sequence?

Part Number: C2000WARE


I have a BLDC motor, it has 3 hall sensors in 120 degree position. i tested hall sensor sequence is:  110,010,011,001, 101,100,    and in reverse direction, the hall sensor sequence is 001,011, 010,110,100, 101.  pls help check if these sequence are correct or not?    

if the hall sensor sequence is correct, what PWM  sequence I need to give to the motor   in both direction?   

thanks