This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: tms320f28035

Part Number: TMS320F28035

Hi all,

I think there is a bug in CLA debugging mode .. Am I right?

I programmed CLA app code to stop; at  '__mdebugstop() ;' and ran it.

CLA debugger stopped at the instruction as commanded and after that, I gave a single step continuously although MSTOP was already reached

and then, I noticed It didn't enter the CLA task anymore unless I reset the CPU ...

many thanks

  • Due to US holidays, you can expect a response by 4'th Dec.

  • The task will need to be triggered again in order for the task to run again. 

    How is the task being triggered?

  • Hello,

    I wanted to see if you had any additional information or if the problem has been resolved?

    Thank you

    Lori

  • Hi Lori, sorry for it.

    I am on vacation now so I will let you know how It works again after I come back to work! 

    thanks for your sincere support! 

  • Hi Lori 

    I have just come back to work.

    I have recorded this video about what I have noticed and been curious about.

    the video shows that I do resume a couple of times and then give single steps to the end of the CLA task.

    when I keep giving a 'single step' a couple of times more although it already reaches to the end of the CLA task, a message in red is shown in the Console window of CCS (please refer it at '00:26' of the video.)

    after I get this message I press the 'Resume' button again. however this app program doesn't stop at ' __mdebugstop();' instruction anymore.

    instead, I get the message saying " Can't run Target CPU : (Error ...) Requested operation cannot be done ....".(please refer it at '00:35' of the video.)

    I have made you wait so long. I apologize for it Lori.

    But I really appreciate your sincere support!

  • I believe this scenario matches one of the special cases documented in the Technical Reference Manual (TRM).  Please try the instructions in the following section of the TRM:

    Debugging CLA Code   ......  special case: MPC halts at or after the MSTOP with no task pending 

    In the current version of the TMS320F28035 TRM this is on page 553.

    Best Regards

    Lori