This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDXIDDK379D: FCL test issue

Part Number: TMDXIDDK379D
Other Parts Discussed in Thread: LVSERVOMTR, C2000WARE

Tool/software: Code Composer Studio

Hi expert,

I tested the FCL code using TMDXIDDK379D and LVSERVOMTR.

CCS version

Version: 9.2.0.00013

SDK version

C2000Ware_MotorControl_SDK_2_01_00_00

Example code

fcl_f2837x_tmdxiddk

Control Card

F28379D controlCARD

Just under build level3, I followed the instructions and everything goes well.

First run, 

After setting fclclrcntr=1

And I want to check the GPIO toggle just like below, describe in this file:fcl_sensored_pmsm_iddk_users_guide.pdf

However, I can only see the pulse of GPIO18 not GPIO16.

I also Change to open GPIO16 to toggle in fcl_cla_code.cla, but nothing changed.

It showed like this.

I tried to connect CLA core and load symbol, but nothing happened.

I want to know where I did wrong.

BR

Emma