Tool/software: Code Composer Studio
Somebody can help me posting an example code where scia and scib are linked?
i would like to see them comunicate :)
thanks for the help
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Somebody can help me posting an example code where scia and scib are linked?
i would like to see them comunicate :)
thanks for the help
Due to US holidays, you can expect a response by 3'rd Dec.
hi,
Currently we don't have an example that has SCI A and SCIB communicating with each other.
We only have example showcasing echoback with serial terminal ,SCI loopback w/ and without FIFOs and interrupts.
Please use the SCI loopback example as reference and split the TX for SCI A and RX for B and comment out the internal loopback.
Regards.
i have done it but it doesn't work...:(
i need not a comunication between scia a and scia b but only only one between these (scia a or scib) for transmit and read with an arduino using 2 pins different from 42 43.
the problem is that no example code with 2 different pins as 42 43 work...
somebody can help me:(
thanks
hi,
francesca rossi said:the problem is that no example code with 2 different pins as 42 43 work...
That'e because the example are written for either the controlcard / launchpad & the board has the FTDI and circuitry to connect only these 2 GPIO pins to the usual USB cable .
If you need to use other 2 pins and view on the PC through USB , you would need to use some external cable connections like the RS232 cable or a USB to UART converter cable and map it to the GPIO that you want to use.
But i guess in this case you are only talking to the arduino..
francesca rossi said:i have done it but it doesn't work
Which board are you using ?
How are you connecting the GPIOs of C2000 board to arduino ?
Are the basic example working fine ? like the echoback etc ?
Regards.