This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: When will the TMS320F2838xD ESC erratas be improved?

Part Number: TMS320F28388D

Hi experts,

Are there any plans to improve the following erratas?
If there is a plan, when will it be improved?

ESC: EtherCAT Slave Controller may not Work with a Non-Gigabit PHY

ESC: The CPU1 DMA Access is Only Available to the Lower 4KB of the ESC RAM Memory Map

Best regards,

Sasaki