Part Number: TMS320F28075
Dear support,
I have 2 peripherals connected to the my TMS320F28075 to the same PWM (PWM11).
One to the A (gpio20).
One to the B (gpio21).
I need to configure them to different frequency (200Hz and 1000Hz).
Is it possible? Both of them share the same TBPRD register...
By playing with the CMPA/B registers, I can set different duty cycle to A and B, but the frequency is common for both of them.
Thanks in advance,
Alex.