This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377D: redefining CLAscratch section?

Part Number: TMS320F28377D

Tool/software: TI C/C++ Compiler

Dear readers,

I'm having 1 software project for two CPU cores so I only need to flash 1 CPU core with 1 firmware file for the entire controller.

I've divided the FLASH in pages for specific code sections which are copied through the IPC to the right RAM area (CPU1, CLA1, CPU2 and CLA2).

That all works just fine, i'm only running into some difficulties with the CLAmath library and things could be done more easy if I could redefine some sections for CLA2

like for the 2nd CLA renaming the  CLAscratch -> CLA_2scratch

Is this possible?

Or maybe it's possible to put all the sections of CLA sources in folder to a specific page (   CLA_RAM: {  projectfolder/dir/*.obj(CLAscratch)   }

Or some other advanced techniques

Best regards,