Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Hi,
I am using this microcontroller to control two power converters, each one with each CPU and its CLA. The CPUs are in charge of the communications and the state machine, while the CLAs execute the control loops of the converters.
My problem is that the CPU1 resets itself without order or apparent cause, but the CPU2 does not reset. Firstly, I programmed everything in both RAMs, and I was able to know that CPU1 reset because it returned to main () (before the while(1)) and it tried to run the program again and when it reached the EINT; instruction it reset again and again. I took a look into the RESC register and the only bit set (apart from the TRSn and XRSn bits) was the WDRSn, but I never configured the watchdog, indeed I always disable it. Then, I realized that sometimes when a program the microcontroller this bit is set from the beginning. I also took a look into the NMIFLG register of the CPU2 but everything seemed fine, all the bits were cleared. The problem was random, maybe one day it happened two times and the next two did not happen. I have to say also, that the problem always happen when the converter was running, it has never happened when the converter was in standby without switching. Could it be something related with electromagnetic interferences?
Having all these problems and thinking that it was due to a problem in the .cmd, I changed it and now I am programming in FLASH but this time the problem is a little different because CPU1 loses control and it seems that it has no program. At some time, when switching and testing the converters, it luckily open the switches, but its output GPIOs start to change constantly; and moreover, when I am debugging, all the variables have random values changing constantly and when I try to stop the program to know what is happening, the CCS says that there is no symbol in this CPU. What may the problem be? Could it be some power supply error?
I always debugged the code without the Real-time mode. I tried to debug enabling it, but the code stopped and I got the error -1142 (see the image below).This time, the converter stopped in an unwanted and dangerous way, and I decided not to try to repeat the error.
Best regards,
Lucas B.