Part Number: TMS320F2801
Hello everyone
I am trying to program a 320F2801PZA device with CCSV8.3. I found an example project from www.ti.com/.../sprc191, which is built to use in a 320F 2808 device.
1. Is it ok to use 2808 code in a 2801 device. ?
2. code compiled successfully, but when ccs try to load the program it says following line in the terminal and fail. why is that?.
3. Note that it also says configured device (TMS320F2801), does not match the detected device, which is wierd because the TMS320F2801PZA is printed on the CPU. How can i know which device is detected by CCS?. target config source code is included below.
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS100v2 USB Debug Probe_0">
<instance XML_version="1.2" desc="Texas Instruments XDS100v2 USB Debug Probe_0" href="connections/TIXDS100v2_Connection.xml" id="Texas Instruments XDS100v2 USB Debug Probe_0" xml="TIXDS100v2_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS100v2 USB Debug Probe_0">
<instance XML_version="1.2" href="drivers/tixds100v2c28x.xml" id="drivers" xml="tixds100v2c28x.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="TMS320F2801_0" href="devices/f2801.xml" id="TMS320F2801_0" xml="f2801.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>
This is the terminal window text
C28xx: Failed CPU Reset: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: GEL: Error while executing OnReset(1): Target failed to read register ST1
at (ST1&~(0x0100)) [f2801.gel:257]
at C28x_Mode() [f2801.gel:38]
at OnReset(1)
C28xx: Flash Programmer: Warning: The configured device (TMS320F2801), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: Failed CPU Reset: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: GEL: Error while executing OnReset(1): Target failed to read register ST1
at (ST1&~(0x0100)) [f2801.gel:257]
at C28x_Mode() [f2801.gel:38]
at OnReset(1)
C28xx: Trouble Writing Memory Block at 0xae0 on Page 1 of Length 0x1: (Error -1137 @ 0xAE1) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE0@Data
C28xx: Trouble Writing Memory Block at 0xae1 on Page 1 of Length 0x1: (Error -1137 @ 0xAE2) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE1@Data
C28xx: Trouble Writing Memory Block at 0xae2 on Page 1 of Length 0x1: (Error -1137 @ 0xAE3) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE2@Data
C28xx: Trouble Writing Memory Block at 0xae3 on Page 1 of Length 0x1: (Error -1137 @ 0xAE4) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE3@Data
C28xx: Trouble Writing Memory Block at 0xae4 on Page 1 of Length 0x1: (Error -1137 @ 0xAE5) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE4@Data
C28xx: Trouble Writing Memory Block at 0xae5 on Page 1 of Length 0x1: (Error -1137 @ 0xAE6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE5@Data
C28xx: Trouble Writing Memory Block at 0xae6 on Page 1 of Length 0x1: (Error -1137 @ 0xAE7) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE6@Data
C28xx: Trouble Writing Memory Block at 0xae7 on Page 1 of Length 0x1: (Error -1137 @ 0xAE8) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error occurred during flash operation: Target failed to write 0x00000AE7@Data
C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: C:\Users\VEGA_1010\Documents\CcsWork2\Example_2808_Flash\Debug\Example_2808_Flash.out: Load failed.