Part Number: TMS320F28335
Other Parts Discussed in Thread: ADS1278
Hi Team,
Is it possible to give clock from same crystal to DSP TMS320F28335 and ADC ADS1278 ?
Thanks & Regards,
Sachin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
Other Parts Discussed in Thread: ADS1278
Hi Team,
Is it possible to give clock from same crystal to DSP TMS320F28335 and ADC ADS1278 ?
Thanks & Regards,
Sachin
Sachin,
There are 2 factors here, one of which I will ask for another team member to comment.
1st factor is that the crystal (X1/X2) input to the F28335 is 1.8V level signal. Reading the ADS1278 DS, it looks like IO range is 1.8 to 3.3V; so if you are using in the 1.8V range this should be OK>
2nd factor is now discussion driving a CLK input on the ADC device with the output of the F28335 internal oscillator circuit; and this is where I willl need to research if there is any impact to our (C2000) oscillator circuit by adding another clock input load.
Finally, if you meant driving both devices with a canned oscillator(using XCLKIN on F28335) where the oscillator circuit is external to both devices, that should be OK.
Best,
Matthew
Hi Sachin,
To add to what Matt said, if you mean a quartz crystal, then no, you can't share it between 2 devices. A quartz crystal and electrical oscillator circuit (inside the F28335 device) will form a closed loop system that should not be driven by anything else.
Moreover, a quick scan of the ADS1278 datasheet shows it does not support a quartz crystal and you can only feed it a single-ended clock from like a can oscillator. You can share the output from a single-ended oscillator among 2 devices but for a more robust design, you might have to buffer the split clocks going to both devices.