Part Number: TMS320F28035
What is the recommendation to connect the VREFHI (80pin package/ unmuxed pin) when using the ADC with internal REF.
Is in this case connection to VSSA without 1kOhm resistor okay like for an unused ADC?
Regards Bernd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035
What is the recommendation to connect the VREFHI (80pin package/ unmuxed pin) when using the ADC with internal REF.
Is in this case connection to VSSA without 1kOhm resistor okay like for an unused ADC?
Regards Bernd
Bernd,
This datasheet recommendation allows for a direct connection to VSSA:
There is no functional requirement to connect unused pins like VREFHI to VSSA when not used; it is a recommendation to help simplify PCB design decisions. As such, I would personally prefer to connect VREFHI to VDDA so that there is an alternate ADC reference source that can be useful as a redundancy and diagnostics.
-Tommy