Part Number: TMS320F280049C
On the TMS320F280049C are the CLB registers accessible by the CLA and the CPU, or only by the CPU?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049C
On the TMS320F280049C are the CLB registers accessible by the CLA and the CPU, or only by the CPU?
Thanks Nima. I did see the above thread before posting my question, but it is specific to the F28379D. I want to know about the F280049C.
The information from TI documentation tends to support that the CLB is accessible from the CLA, at least for some devices. In one CLB application report it states several times that the CLB can be accessed by either the CPU or the CLA (http://www.ti.com/lit/an/spraco2/spraco2.pdf ). The technical manual for the F2838x clearly states that the CLA can access the CLB (http://www.ti.com/lit/ug/spruii0a/spruii0a.pdf e.g. Table 9-13 page 1147). However, the datasheet and technical manual for the F280049C gives no guidance about whether the CLA can access the CLB.
Please can TI produce a table or list showing which devices support CLA to CLB access and which do not.
Thanks for your continuing support.
Yes for F28004x, CLA has access to CLB.
I will update the other thread with F2837x specific answer.
Nima