Part Number: TMS320F2808
Other Parts Discussed in Thread: TI-API
Hello,
after manufacturing test of boards some of the boards showed strange behaviour after the test sequences. In such cases, the two TMS320 devices became locked. The root cause is currently unknown.
In order to track the problem further, we implemented various CMSSCR read procedures into the test flow.
Before programming: 0050H
After programming: 0070H
This is true for all variants of this board and also for other boards using the same TMS320 device.
Now the question:
When reading the CSMSCR register of some other boards, we see CSMSCR values:
DSP1 = 0047H
DSP2 = 0041H
But they should be 0050H... What do these values mean? Is there a table describing the values further?
Many thanks in advance!