Hi. I've designed my own PCB that uses the F2808 Control Card. I have a 2 internal power planes, GND, and 5V. Each power pin from the DIMM connector goes straight to the power or GND plane. When I apply 5V to the board, the controller works randomly. I will either have problems when I power the board, or when I try to debug it with CS4. However, if I lower my 5V supply to around 4V, I don't have any issues at all. The only difference between my board and the evaluation boards is that I route the 5V pins directly to the power plane.
Any suggestions?
Thanks,
Omer Peleg
Data Technologies Inc.