Part Number: TMS320F28335
Hello,
For a tms320f28335 I generated the .bin file from the .out file by using the hex2000 tool because I am debugging a release version. The size of the .bin is 40kbytes but after the address 0x2200 the .bin image is filled up with 0 and it does not seem to have code instructions. From what I can see from the map file, the real size should be much lesser (just around 0x2200 or so). Am I missing something or this is a correct size?
Thanks and regards