This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Launchpad Suddenly dead

Part Number: LAUNCHXL-F28379D

Hi,

The launchpad suddenly went irresponsive when working and it is no more working. The LEDs are no more light when connected to PC and no more able to build from Simulink. Following error shows while building in Simulink.

SEVERE: IcePick_C_0: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged in, invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. (Emulation package 8.2.0.00004) SEVERE: emulation failure occurred SEVERE: Error connecting to the target: emulation failure occurred *** Cannot create a valid debug session for Board/CPU=*/C28xx_CPU1. Make sure this matches only one board and one CPU. Exiting...

 

Update:


I think some shortcircuit happened. Not sure. The voltage at 3.3V rail is not proper, its around 0.4V. I have removed JP1 jumper and D4 Led turns ON.

Simulink error is 

SEVERE: IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.2.0.00004)