Part Number: TMS320F28069F
Hello!
I have an Instaspin FOC based application. It runs the Speed Control lab correctly and now I have to develop the failures detections to avoid dangerous situations (e.g: loss of CAN comms, ...). One of the things to be verified is that the inverter has the motor connected. I have seen that if you run the lab 3b with no motor connected the given estimated speed is nearly equal to the reference speed during 3 -5 seconds (fake) and then it goes to a high (random?) values. Is there any way to detect this absence of motor? Now I just verifying that after some time both speed and torque values (filtered) are coherent. I don't know if this is the best way to do that? How can I avoid these fake values?
Thank you in advance
Borja Gómez