Other Parts Discussed in Thread: C2000WARE
Hello Expert,
Our customer is now evaluating the CAN interface on F280049.
They recognized they can dynamically change the TX object by referring "26.12.5 Changing a Transmit Object" in TRM.
Actually, they used CAN_setupMessageObject() for the message setup , then use CAN_sendMessage() for sending which are from C2000 ware library.
They looped this sequence , setup and send, repeatedly, then sometimes TX was not sent which means CAN Analyzer did not receive the data.
Are there the actual result which this type of sequential TX was well performed with no issue?
They did not think that they need the confirmation of some flag out side the functions before the TX,
but if there is something to consider in such a TX loop , please advice.
Reards, A.Fujinaka