This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: getting error WHILE DUMPING eg code frm c2000 in tms320f28388d with help of docking station.

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

in one line my problem is that i m not able to dump the eg code in my device TMS320F38388D with help of Docking station.Below i explain my procedure.

EXPLAINATON:

1) fix my tms320f28388d in docking station

2)power the device with the USB cable, led in both docking station and tms320f28388d start glowing

3)then i follow C:\ti\c2000\C2000Ware_<version>\driverlib\f2838x\examples 

4)i dump eg of LED which is there in my c2000

5) then build>flash 

6)after doing all this i m getting an error which i m displayin you in below screenshot.