This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374S: About EMIF write cycle time

Genius 5840 points

Part Number: TMS320F28374S

Hello,

In datasheet, EMIF write cycle time seems to be following.

MIN: (WS+WST+WH+2)*E–3

MAX: (WS+WST+WH+2)*E+1

My corresponding resister value is following:

W_SETUP: 0011

W_STROBE: 000111

W_HOLD: 000

EM1CLK=99MHz.

Is the formula correct with the following recognition?

MIN: ((3+1)+(7+1)+(0+1)+2)*(10.1ns) - 3=148.5ns

MAX: ((3+1)+(7+1)+(0+1)+2)* (10.1ns) + 1=152.5ns

Regards,

U-SK