This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F280049C: How to program in flash of F280049c

Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

Hello,

I am sourabh working on Launchxl F280049C. I am able to write and execute the code from RAM memory of F280049c board but i am not able to burn the code inside of ROM memory.

Is there any switch settings?

I select CPU1_FLASH from build configuration-> set active-> CPU1_FLASH. but while burn the code i got an error

Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 8.3.0.00003)

please suggest me solution for this.

Thanking you,

Sourabh