Tool/software: Code Composer Studio
Hi there,
I am currently having trouble finding documentation regarding connections required for the USB-UART bridge for the TMDSDOCK28335. I have a jumper connecting both pins of J9, but I cannot connect to the board, any schematic information/ pictures of connections would be very helpful.
I tagged the thread I used to determine the jumper for J9; however, do I simply connect the Rx pin on J3 to GPIO 12 configured for SCI TxDA and the Tx pin on J3 to GPIO 9 configured as SCI RxDA? Or are there further connections required for configuring SCI communication?
Connections between J3 and SCI Tx and Rx, as well as I connected pins V33 to a 3.3 volt pin and GND to GND is that neccissary?
Is this how you connect jumper J9?
Thanks,
Alex