This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Bootloader - Boot Mode Select Pin

Part Number: LAUNCHXL-F28379D


Hello  everyone,

I'm using Bootloader to put the code into the MCU via SCI. I'm using LAUNCHXL-F28379D to take this. I have a problem like this:

I read the Serial Flash Programming of C2000™ Microcontrollers and also read the code from C2000 and I see the code use GPIO84 and GPIO85 as SCITXDA and SCIRXDA (or GPIO29 and GPIO28 for second option). But I can't find them on the LAUNCH board. So i have some following question:

1) Can I change the GPIO pins to run the application??

2) If I run bootloader, I still connect the JTAG for power supply or are there any method for power supply in LAUNCHXL-F28379D???

I run the code F2837xD_sci_flash_kernels in C2000 example for dual core Example Code.

I hope to see your reply.

Best Regard!!