Tool/software: Code Composer Studio
Hello ,
I am using ti launch pad for testing of PWM Sync between two DSP .... I have Two launch pad...... I am using EPWM4 Of one DSP-1 Board as sync signal for Other DSP-2 Board.....
And I am Checking EPWM1A of Both The DSP board On Scope.....Both Board Has Same Duty of 0.75% ..... i am attaching sanpshot of PWM signal....
Yellow one is DSP-1 board EPWM1A PWM pulse.....
Blue One is DSP-2 Board EPWM1A PWM Pulse...
I Am Not able To understand Why Two PWM are not match Exactly to each other ???...
Why falling of Yellow one is match with Rising of Blue one ????.
Why Both the Rising and Falling edge of Two DSP boards is not exactly matching???
i have seen TBSTS register SYNCI bit ..it was set to 1... when EXTSYNCIN1 occurs in Debug mode...