Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: TPS62162
Hi,
I am planning to develop the system based on LAUNCHXL-F28069M operating in stand-alone mode (no Emulator) and executing the program from flash memory. In reference to this, my question is:
Can I use +5 V supply to power the launch pad through mini USB connector of the launchpad ? I will keep jumpers JP1 & JP2 populated.
or do I compulsorily require 3.3 V supply to power the launch pad through connector J9 ?
With thanks & regards,
Dipen