Part Number: TMS320F28069
I am using the TMSDOCK28069 station with TMS320F28069UPZ microcontroller. I am trying to load the proj_resolver01b.ccs project onto the board. The compilation is clear but it stops at line no 175 in proj_resolver01b.c at the following code
#ifdef FAST_ROM_V1p6
ctrlHandle = CTRL_initCtrl(ctrlNumber, estNumber); //v1p6 format (06xF and 06xM devices)
controller_obj = (CTRL_Obj *)ctrlHandle;
#else
ctrlHandle = CTRL_initCtrl(estNumber,&ctrl,sizeof(ctrl)); //v1p7 format default
#endif
Break at address "0x3fa6fb" with no debug information available, or outside of program code.
How do I solve this problem??