Part Number: TMS320F28075
Other Parts Discussed in Thread: C2000WARE
Hello,
I managed to compile and run the "usb_ex1_serial_device" project from latest version of C2000Ware.
The board registers a virtual COM port with provided driver and looks fine on Windows 10 side.
I can send data (in 6 byte packets) from PC using a terminal software and receive it on SCIA-RX pin.
In next step, I connected the SCIA-RX to SCIA-TX on microcontrller (GPIO28 an GPIO29), on terminal software I receive only 2 bytes of sent data whenever I send a packet.
Here is the example:
Tx: "USBSER" Rx: "US"
Tx: "TEST P" Rx: "BS"
Tx "rogram" Rx: "ER"
It seems that the data buffered correctly but the interrup for USB serial TX does not trigger properly.