Folks,
My project is running into release phase, however, I met the performance bottleneck which cause catastrophic fault. I need to optimize the system where possible.
We use F28335 chip, what I have done so far are:
1. reduce random access time and paged access time of internal FLASH
2. run most of real-time code from internal SARAM
are there any practical methods I can leverage to optimize my system?
Thanks
Tim