This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28027: C compiler

Part Number: TMS320F28027
Other Parts Discussed in Thread: CONTROLSUITE

Tool/software: TI C/C++ Compiler

I have F28027 Piccolo board. I have installed Embedded Coder Support Package, Control Suite, and CCSv6. Also in Matlab 2017b, simulink model configuration in hardware implementation section I have selected board. But when I build model (Ctrl+B) I get the following error: 

---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

 Build 

  1
02:11 PM Elapsed: 11 sec
### Starting build procedure for model: Blink ### Generating code and artifacts to 'Model specific' folder structure
  Code Generation 
 3
Elapsed: 9 sec
### Generating code into build folder: C:\Users\Sanjeev Gupta\Documents\MATLAB\project\Blink_ert_rtw ### Invoking Target Language Compiler on Blink.rtw ### Using System Target File: C:\Program Files\MATLAB\R2017b\rtw\c\ert\ert.tlc ### Loading TLC function libraries ### Initial pass through model to cache user defined code . ### Caching model source code ### Writing header file Blink_types.h ### Writing header file Blink.h ### Writing header file rtwtypes.h ### Writing source file Blink.c . ### Writing header file Blink_private.h ### Writing source file Blink_data.c ### Writing header file rtmodel.h ### Writing source file ert_main.c ### TLC code generation complete. ### Evaluating PostCodeGenCommand specified in the model
  Code Composer Studio Project 
 1
Elapsed: 0.509 sec
### Creating CCS Project at : C:\Users\Sanjeev Gupta\Documents\MATLAB\project\Blink_ert_rtw\CCS_Project ### CCS project created successfully Open project in Code Composer Studio.
### Using toolchain: Texas Instruments C2000 Code Generation Tools v16.9.2 | gmake (64-bit Windows) ### Creating 'C:\Users\Sanjeev Gupta\Documents\MATLAB\project\Blink_ert_rtw\Blink.mk' ... ### Building 'Blink': "C:\PROGRA~1\MATLAB\R2017b\bin\win64\gmake" -B -f Blink.mk all C:\Users\Sanjeev Gupta\Documents\MATLAB\project\Blink_ert_rtw>cd . C:\Users\Sanjeev Gupta\Documents\MATLAB\project\Blink_ert_rtw>if "" == "" ("C:\PROGRA~1\MATLAB\R2017b\bin\win64\gmake" -B -f Blink.mk all ) else ("C:\PROGRA~1\MATLAB\R2017b\bin\win64\gmake" -B -f Blink.mk ) C:/PROGRA~3/MATLAB/SupportPackages/R2017b/3P.instrset/tic2000codegentools.instrset/ti-cgt-c2000_16.9.2.LTS/bin/cl2000 --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SupportPackages/R2017b/3P.instrset/tic2000codegentools.instrset/ti-cgt-c2000_16.9.2.LTS/include" -v28 -ml -DMODEL=Blink -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=4 -DSTACK_SIZE=512 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DDAEMON_MODE=1 -DMW_PIL_SCIFIFOLEN=4 -DSTACK_SIZE=512 -DRT -DMODEL=Blink -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/Users/Sanjeev Gupta/DOCUME~1/MATLAB/project -IC:/Users/Sanjeev Gupta/DOCUME~1/MATLAB/project/Blink_ert_rtw -IC:/PROGRA~1/MATLAB/R2017b/extern/include -IC:/PROGRA~1/MATLAB/R2017b/simulink/include -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2017b/rtw/c/ert -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tic2000/src -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/supportpackages/tic2000/inc -IC:/ti/controlSUITE/device_support/f2802x/v230/f2802x_common/include -IC:/ti/controlSUITE/device_support/f2802x/v230/f2802x_headers/include -IC:/ti/controlSUITE/device_support/f2802x/v230 -IC:/ProgramData/MATLAB/SupportPackages/R2017b/toolbox/target/shared/externalmode_daemon/include --output_file=MW_c28xx_board.obj MW_c28xx_board.c [project.] >> WARNING: more than one source file is specified; option --output_file is ignored Fatal error: cannot open source file "Gupta/DOCUME~1/MATLAB/project" 1 catastrophic error detected in the compilation of "Gupta/DOCUME~1/MATLAB/project". Compilation terminated. >> Compilation failure gmake: *** [MW_c28xx_board.obj] Error 1 C:\Users\Sanjeev Gupta\Documents\MATLAB\project\Blink_ert_rtw>echo The make command returned an error of 2 The make command returned an error of 2 C:\Users\Sanjeev Gupta\Documents\MATLAB\project\Blink_ert_rtw>An_error_occurred_during_the_call_to_make 'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command, operable program or batch file. ### Creating HTML report file Blink_codegen_rpt.html
### Build procedure for model: 'Blink' aborted due to an error.
Error(s) encountered while building "Blink": ### Failed to generate all binary outputs.

 ---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------