Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TMS320F28379D, C2000WARE
Hi,
I purchased a LAUNCHXL-F28379D which has TMS320F28379D inside. I'm trying to configure pins of MCU for PWMs,ADCs,SCI,CAN,GPIO etc.
I checked the datasheet of TMS320F2837xD Dual-Core Delfino™ Microcontrollers at page 41 for pin multiplexing.
1.) I couldn't see the ADCIN14 and some ADC ports at the "Table 4-3. GPIO Muxed Pins". How can i find it in order to send some registers to my code.
2.) Actually, I couldn't understand which pins are disabled when I chosed some configurations. As an example, i'm worndering that if I configure in order to use EPWM1A, EPWM1B, EPWM2A, EPWM2B,
can I still use GPIO0 and SCITXDB,SCIRXDB,CANRXB,CANTXB?
3.) If I configure according to use EPWM1A, EPWM1B, EPWM2A, EPWM2B, is the only available SCI ports are SCITXDA,SCIRXDA for this register?
I attached the table as below.