This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320LF2406A reset rise time

Hi, we have a situation wherein we'd like to put a rather large capacitor on the RS pin of the '2406 DSP (pin 93, LQFP-100 package). I've looked quite a bit for a specification on maximum rise time of the reset signal, but can't find one. Is there any reason to be concerned if the rise time exceeds, say, 100 us - 1 ms on the reset signal?

Regards.  --Todd