Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Hello,
I´m working with the F28379D and I want to include the CLAmath library in my project. Following the description I have to include the ROM symbols table from the folder:
C:/ti/c2000/C2000Ware_x_xx_xx_xx/libraries/boot_rom
This folder contains two revisions (rev0 and revB).
Which revision has to be used?
Both revisions contains two symbols folder (c1_CLA_Data_ROM and c2_CLA_Data_ROM).
Which folder must be used and what is the difference between c1_CLA.... and c2_CLA…..?
In order to check the using of the data ROM I have to check the addresses of the ROM tables in the map-File. Where can I found the addresses of the CLA data ROM in the TRM?
Best regards
Ralf