This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Code Library Support for SVN and BiSS-C for the F28388D

Part Number: TMS320F28388D

Is there or is there a plan to have Library Code support for SVN (Space Vector Modulation) and/or BISS-C (encoder communication) for the F28388D?

If so, when? 

  • I believe the MotorControl SDK contains a few SVGEN modules you can use for space vector modulation. We do not currently have a BiSS-C library for F28388D but it is planned. If you check back with us toward the end of this quarter we could be able to give you more details.

    There is a library already available for the F2837xD although it can't be reused on the F2838x. This thread below does suggest that you might be able toimplement the logic for BiSS-C for the F2838x using the CLB  on your own if it's needed sooner than we can provide it

    Whitney