Other Parts Discussed in Thread: TMS320VC5507
Hello
I am writing a thesis on studies.
I use ADS1672EVM-PDK
I need to send in Code Composer Studio a start signal to ADS and gather the probs.
I need to send a star command.
I thinkt that I should do it by putting the start pin in ADS to high state and than to low.
I need to do it by the microcontroller. But I am not sure which pin of tms320VC5507PGE is connected to ADS. I think that 125 pin (FSX), but when I check it with multimeter, I can not say that there is a signal betwen them.
I need help to be sure which pin should I put into high state and I need a command to do it.
I had been looking for tms320vc5507 command set but I didn't find it.
I tried to see how does the proram of blinking led wokrs, and also I don't see any command to put high and low state of pin.
I need to know where can I find those commands or please tell me what is that command.
I need to know also which pit is the start one.
Please help me. I am newbie :)