Other Parts Discussed in Thread: UNIFLASH
Hello,
I am flashing TMS20F2806 using above uniFlash. I want the DSP to boot from flash and hence BOOT config pins are all set to high --> GPIO 18, 29 and 34
I am using a emulator XDS200 USB to program the DSP.
Once I load the program, I get a message saying Program load completed successfully.
I use below settings:
1. Flash program settings: Erase, program, verify
2. Clock: OSCCLK: 20MHZ, CLKINDIV: 2, PLLCR: 10
3. Erase sector Selection: All sector A, B, C, D are clicked
4. Password is correctly entered - Code security password Key 7 to Key 0
How I program?
1. Browse flash image
2. Click Load image
3. I get a message saying Program load completed successfully
4. Then I click verify image
5. I get error message: Verification failed at address 0x3F0000
Can someone help me on this?