This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: High Frequency Inverter Output Failed

Part Number: TMS320F28379D


I'm working with building an induction heating system using TMS320F28379D as micro-controller for single phase inverter. But controller board gets turned off when receiving high frequencies from inverter output (more than 500Hz). But I need minimum 20kHz output AC signal from inverter. Please help how can I configure this control board? Or is there any other suitable control to do this easily?