Part Number: TMS320F280049
Hi;
Are all the GPIOs pins of F280049 interrupt-able by an external hardware?
Specifically: GPIO1, GPIO15, and GPIO23.
Thanks!
Wen Li
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
Hi;
Are all the GPIOs pins of F280049 interrupt-able by an external hardware?
Specifically: GPIO1, GPIO15, and GPIO23.
Thanks!
Wen Li
Yes, all the GPIO pins can be use as external interrupt source.
Regards,
Vivek Singh
Thanks for the quick response!
Now, I am being specific to my application.
I assume following will work
The GPIO15 is connected to an external temperature sensor. When temperature is higher than a certain degree, the sensor will send a pulse to GPIO15; this event will interrupt the F280049. And the F280049 will enter the interrupt service routine to serve this event.
Is my assumption about the GPIO15 correct?
Wen Li
HI Wen,
Yes, your understanding is correct but you need map GPIO15 to one of external interrupt (XINTx and enable it in corresponding XINTxCR register) via INPUT_XBAR.
Regards,
Vivek Singh