Part Number: TMS320F2809
Other Parts Discussed in Thread: MOTORWARE
I am writing some code to interact with a external peripheral that uses a SPI-like communication. I give it a clock and it gives me data, so I'm using the peripheral as follows:
- Read the data in the SPI's RX FIFO
- Process data
- Fill Tx FIFO
This routine runs at 1khz in the SYS-BIOS. The problem is I run into traces that look like this:
The gap on the top(CLK) trace causes the peripheral to time out and think that the next word is a new transaction.
This is what the code for filling the TX FIFO looks like:
// Fill the FIFO to get new sample ready.
for (int words_needed = 4; words_needed > 0; words_needed--) {
spi_handle_->SPITXBUF = 0xFFFF;
// Wait for buffer to empty
while (SPI_getTxBufferStatus(spi_handle_) == SPI_TxBufferStatus_Full);
}
This isn't atomic, so when interrupted, this filling process can be delayed. What I want to do is put a SPI_disableTx() before then SPI_enableTx() after, but for some reason when you disable TX it doesn't stop the peripheral from clocking which ruins this idea.
Would love some help on this!
Thanks!