This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MOTORWARE: Motor Speed Control

Part Number: MOTORWARE
Other Parts Discussed in Thread: DRV8301

Tool/software: Code Composer Studio

Dear Expertise, 

Working with a University Project , this question is to know whether this idea is possible or not with TI Launchpad F28069M development kit and Boostxl DRV8301 Evaluation module. 

We want to set(change) the motor speed, but not thru code composer studio or any software connected to the launchpad (we want the launchpad to be standalone not connected to any pc), however the launchpad is being connected via analog interface to EV3 LEGO, and the LEGO being directed by MATLAB. So we set the desired speed from the MATLAB -->LEGO-->LAUNCHPAD-->MOTOR. 

This part  LAUNCHPAD-->MOTOR  and this part MATLAB -->LEGO are well know, but the question is, how can we change the motor  speed (forexample  of lab5c ) by an external  input analog PWM  signal , from the interface explained above? (I dont know if we can reach the data speed in another place on the CPU, it would be good if you direct us). 

I dont know if I was clear, I know TI dont have enough knowledge about LEGO I have searched for this question before, We just want to know how this step can be done ? 

It would be nice to have a reply before the weekend. 

Best Regards,