This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Load program into FLASH using SCI

Part Number: TMS320F28377S


Hello, guys!

I need your help one more time...

Is there a way to use SCI interface to load program into FLASH? Or JTAG is the only way?

I need a way to use a serial interface (something like RS232) to burn the .hex file into FLASH in my production line, so I can use an already existing structure.

Is it possible? Is JTAG the only way to burn .hex into FLASH? What do you suggest?