Other Parts Discussed in Thread: C2000WARE
Dear Team TI,
As shown in attached image,
There appears a glitch because of PWM at output. The glitches are shown in red color text.
The waveform in red is value to be put in EPwm3Regs.CMPA.bit.CMPA value. The pink is output of PWM3 (GPIO 4). The green is ISR probbed at one of the GPIO.
So, the value of CMPA register is changing at the end of ISR (point 1 of image) , so output of PWM should change in next ISR i.e. at point 2 (of image), instead it is changing at point 3 (of image), and hence the delay from point 2 to 3 is appearing in output, which is undesirable.
I have 3 PWMs in the system and out of which PWM 1 is also used for ISR (Freq. of ISR is 10 kHz). I am changing the value of CMPA in PWM1 ISR
The freq.of glitch is 20 kHz.
KINDLY HELP.
Below is how I have defined 3 PWMs.
void InitEPwm1()
{
EPwm1Regs.TBPRD = 5000; // Set timer period for 10KHz
EPwm1Regs.TBPHS.bit.TBPHS = 0x0000;
EPwm1Regs.TBCTR = 0x0000;
//
// Setup TBCLK
//
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
EPwm1Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
//
// Setup compare
//
EPwm1Regs.CMPA.bit.CMPA = 2500;
//
// Set actions
//
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm1Regs.AQCTLA.bit.CAD = AQ_SET;
EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.CBD = AQ_SET;
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;
EPwm1Regs.ETSEL.bit.INTEN = 1;
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST;
}
//
// InitEPwm2Example - Initialize EPWM2 configuration
//
void InitEPwm2()
{
EPwm2Regs.TBPRD = 5000;
EPwm2Regs.TBPHS.bit.TBPHS = 0x0000;
EPwm2Regs.TBCTR = 0x0000;
//
// Setup TBCLK
//
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
//
// Setup compare
//
EPwm2Regs.CMPA.bit.CMPA = 5000;
//
// Set actions
//
EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm2Regs.AQCTLA.bit.CAD = AQ_SET;
EPwm2Regs.AQCTLB.bit.CBU = AQ_CLEAR;
EPwm2Regs.AQCTLB.bit.CBD = AQ_SET;
}
//
// InitEPwm3Example - Initialize EPWM3 configuration
//
void InitEPwm3()
{
EPwm3Regs.TBPRD = 5000; // Set timer period for 10KHz
EPwm3Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0
EPwm3Regs.TBCTR = 0x0000; // Clear counter
//
// Setup TBCLK
//
EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up DOWN
EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE;//TB_ENABLE; // Disable phase loading
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm3Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
EPwm3Regs.TBCTL.bit.PHSDIR = TB_UP;// already set correctly
EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO
EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
//
// Setup compare
//
EPwm3Regs.CMPA.bit.CMPA = 2500;
//
// Set actions
//
EPwm3Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set PWM3A on Zero
EPwm3Regs.AQCTLA.bit.CAD = AQ_SET;
EPwm3Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM3A on Zero
EPwm3Regs.AQCTLB.bit.CBD = AQ_SET;
}