Part Number: TMDSCNCD28069MISO
Other Parts Discussed in Thread: CONTROLSUITE
Using controlSUITE, I have been inspecting the reference design for the Piccolo F2806x DIM100 controlCARD w/ Isolated Emulation. The file name for the schematic is "f2806x iso-controlcard0.4-sch.pdf". On the second page there is a schematic showing a USB B-Mini port for M1 below the micro-controller. Does this device appear in hardware on the controlCARD? I can see two other USB ports on the other sheets which are clearly implemented on the TMDSCNCD28069MISO controlCARD hardware.
Not sure what I should be doing with that M1 device and its connections if I would use this as a reference design.
Any clarification here would be appreciated!
John