This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: PUMPREQUEST register has 2 definitions in the TRM

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

I'm confused about the flash pump semaphore register. In the TRM, the PUMPREQUEST register is said to be part of a register file called FLASH_PUMP_SEMAPHORE_REGS but I can't find it in the header files.

Furthermore its base address is 0x0005CE24 but this address is located in the IPC register memory range, and documented in the same TRM (under the same name) as part of CPU1TOCPU2_IPC_REGS_CPU1VIEW.

Should I forget about the "flash pump semaphore registers" and simply use the IPC definition?

Pierre