Part Number: TMS320F280049
Hi all,
Recently, Our product meet a problem about Local Interconnect Network Module of TMS320F280049. And the LIN chip we have used is NXP TJA1021. When the supply voltage of the LIN chip circuit happen the voltage sags( supply voltage:12V sag to 6V (and last 2ms)),the communication will cut off immediately with the occurrence of undervoltage. The voltage sag to minimum 4.1v < the undervoltage protection point of LIN chip(NXP TJA1021) 4.7v.
My issue is when this kind of case happen,why the LIN Module of DSP will stop working. And the voltage sags only last 2ms. when the supply voltage become correctly, why the LIN Module of DSP will not recover ?and which interrupt will happen in this case?
Best wishes, It is apprciated if you could give us a reply on this matter as soon as possible.
YJ