This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Embedded Coder Support Package

Part Number: TMS320F28388D

Hello,

we are looking forward to begin developing a Motor Drive application based on the F28388D processor and we would like to do the programming via Simulink (Embedded Coder). At this moment there is only a reduced support of the processor in the Embedded Coder Support Package, so the question is: is it planned in the near future to provide blocks for the CPUx - CM IPC interface and Ethernet communication? Do you have maybe a roadmap about what will be included in future releases?

Best Regards,

Roberto.

  • Hi Roberto,

    We do not publish development roadmaps at MathWorks.

    However, I can tell you we are actively working on filling in the gaps for our support for F2838xD. Substantial features are scheduled for the next 2 releases: R2020a in the Spring, and R2020b in the Fall. IPC interface & Ethernet support are both on our list.

    If you can work with F28379D for now, the support for F2838xD will be much more complete after R2020b.

    If you need more info, please DM me directly and we can discuss further - additional disclosures may require an NDA.

    Cheers,

    -Brian

  • Hi Brian,

    thanks a lot for the information! I will be contacting you directly.

    Best Regards,

    Roberto.