Part Number: DRV8301-HC-C2-KIT
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hi All,
While trying to flash Control Card - CC2803x ISO DIMM using the Code Composer Studio with the PM_Sensorless project from the "C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105", I am getting following warning and an error.
Warning :- This project was created using a version of compiler that is not currently installed - 5.2.10 [C2000]. Another version of the compiler will be used during build - 18.12.4.LTS.
Error:- Load program error. Multiple debuggable cores detected.
How to load this project to this control card? Shall I use the old version of compiler? I couldn't find 5.2.10 compiler for C2000 from TI archive.
Best,
Amit