Part Number: TMS320F2812
Hi,
I am working TMS320F2812 MCU for my pmsm drive. I am facing problem with 3.3V and 1.8V. After testing of some days the micro controller got spoiled. When I checked the resistance between 3.3V and digital ground, it is showing as short. And it is also short with 1.8V and ground. After replacing the F2812 micro controller with new one, it is working fine. when I powered up my control board without micro controller(not stuffed), all other ICs ( example: 3.3V and 1.8V LDO Regulator) are working fine.
Would you please tell me what are the possible cases for the micro controller failure with the above mentioned scenario?
I am using following IC for the generation of 3.3V and 1.8V from 5V supply.
TPS767D318 - 3.3V
TPS73219DBVR - 1.8V
Thanks & Regards,
Siva.