Hello everyone,
I'm doing my project using Bootloader in TMS320F28379D Launchpad. I know that It seems hard to use SCI Bootloader using this Launchpad because of the lack of necessary pins. So I decided that I use Flash Boot Mode to do this. This is what I am doing: I transfer the code via SCI and then put it into the FLASH sector A. Is it possible to follow my way?
If yes:
1) How can I enter in Flash boot mode? I viewed example code F2837xD_sci_flash_kernels, but I don't know how can I enter in other boot mode. Please guide me !!
2) How Can I write my application code into a sector which is different from Bootloader-sector?
3) How can my application code run right after my firmware update?
If no: Can you show me some way to do my project with this? I have to use this Launchpad to do my project. I really need your help so please reply as soon as possible.
Thanks,
Best regard,