This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2809: Upgrade to add WiFi

Part Number: TMS320F2809

Have an existing TMS320F2809PZ design with almost all pins used.   Need to upgrade to newer device with more flash&RAM and add WiFI capability yet remain somewhat software compatible.   What are the most recent parts that I can use to minimize the chance of going obsolete?   Need 120 to 160 pin range, double the flash to 512K, 34K RAM or larger, 12b X 16 A/D, CAN bus required.  Current options

TMS320F28335ZJZQ

TMS320F28335PTPQ

TMS320F28235PGFA

I am concerned that the datasheet for this device is from 2007...   Are these a good choice for redesign to add WiFI capability?